USB Multilink ML-12 RevC,  new Vista machine,  Hiwave cant find it.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Multilink ML-12 RevC,  new Vista machine,  Hiwave cant find it.

Jump to solution
2,601 Views
TurboBob
Contributor IV

had some errors when installing the drivers.  Did searches of the PE micro and Freescale site and found a few guys with the same problem, but no solutions were posted in the threads.

 

I have done the usual Windoze dance (uninstall, reboot, reinstall) with no change.

 

Anyone here using Vista (32 Home Premium) successfully?

 

CW 6.2  freshly downloaded.

 

Bob

Labels (1)
0 Kudos
Reply
1 Solution
928 Views
TurboBob
Contributor IV


I got it to work after several long, wasted days of messing with it.  I was ready to roll back to XP but that would have been weeks of work.

This is from memory,  but it should be close.

install driver.  it fails.

reinstallations fail on a 'can't find file' error.

plug USB-ML12 into computer.

open device manager, under Jungo you will see one entry for the multilink (there are supposed to be 2)

in c:\pemicro\drivers edit the windrvr6.inf file  find the line below and put a ; at the beginning

windrvr6.sys,,,0x22  ; COPYFLG_NOSKIP | COPYFLG_NO_VERSION_DIALOG

now looks like:
;windrvr6.sys,,,0x22  ; COPYFLG_NOSKIP | COPYFLG_NO_VERSION_DIALOG

save the file.


in the device manager,  right click the top node (the name of your computer) and select "install legacy hardware"
click search for hardware, let the computer search and give up.  Then select browse for driver, navigate to C:\pemicro\drivers\windrvr6.inf

click ok, the computer will complain that its not a digitally signed driver,  click install anyway

the installation will complete and in the Jungo section of device manager there will be 2 entries.

The USB_ML12 will now work

View solution in original post

0 Kudos
Reply
1 Reply
929 Views
TurboBob
Contributor IV


I got it to work after several long, wasted days of messing with it.  I was ready to roll back to XP but that would have been weeks of work.

This is from memory,  but it should be close.

install driver.  it fails.

reinstallations fail on a 'can't find file' error.

plug USB-ML12 into computer.

open device manager, under Jungo you will see one entry for the multilink (there are supposed to be 2)

in c:\pemicro\drivers edit the windrvr6.inf file  find the line below and put a ; at the beginning

windrvr6.sys,,,0x22  ; COPYFLG_NOSKIP | COPYFLG_NO_VERSION_DIALOG

now looks like:
;windrvr6.sys,,,0x22  ; COPYFLG_NOSKIP | COPYFLG_NO_VERSION_DIALOG

save the file.


in the device manager,  right click the top node (the name of your computer) and select "install legacy hardware"
click search for hardware, let the computer search and give up.  Then select browse for driver, navigate to C:\pemicro\drivers\windrvr6.inf

click ok, the computer will complain that its not a digitally signed driver,  click install anyway

the installation will complete and in the Jungo section of device manager there will be 2 entries.

The USB_ML12 will now work

0 Kudos
Reply