Trigger A & B occurred??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Trigger A & B occurred??

3,603 次查看
HarrySun
Contributor I
in CW debugger, it sometime shows "Trigger A & B occurred"
what does it mean??
thanks

 
标签 (1)
0 项奖励
回复
3 回复数

1,146 次查看
YeOldeBDM
Contributor III
I have seen this message when the power on the target is interrupted, or the bdm connection is intermittent.
0 项奖励
回复

1,146 次查看
CrasyCat
Specialist III
Hello
 
That message is generated when you have enabled some triggers on the DBG module.
In the connection menu (MultilinkCyclonePro, GDI, .....) select "Trigger Module Settings".
 
There are probably some triggers defined in the Trigger settings tab.
Delete the triggers if you do not want to see the message again.
 
CrasyCat
0 项奖励
回复

1,146 次查看
joerg
Contributor II
Hi
or you have triggered an interrupt but the vector setting is not correct! I.E. there was an TIM OC interrupt but you have forgoten to set the VECTOR x (in the prm file) to your interrupt routine.

Saluti Joerg
0 项奖励
回复