The new MC9S08QG8 demo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The new MC9S08QG8 demo board

9,818 Views
FC
Contributor III
Has anyone used the new MC9S08QG8 demo board ?
Labels (1)
0 Kudos
Reply
7 Replies

1,667 Views
noritan_japan
Contributor I
I am using the demonstration board as ...

a standalone application
http://www.geocities.jp/programmer_noritan/hc08/TaiyouKei/step1.html
三値デジタル太陽計(3-level digital sun-meter)

an expandable base board
http://www.geocities.jp/programmer_noritan/hc08/TaiyouKei/step3.html
二桁表示太陽計(2-digit digital sun-meter)

and a development tool
http://www.geocities.jp/programmer_noritan/hc08/tools/mlinkQG8.html
DEMO9S08QG8評価ボードを開発ツールとして使う
(Use DEMO9S08QG8 demonstration board as a development tool)

It's very good for these purpose.
0 Kudos
Reply

1,667 Views
Cheesehead
Contributor I

Hello FC,

Yes, I have the QG8 Demoboard for some time; had no issues with this after updating my CodeWarrior for the support of the device. Comes complete with Codewarrior and an on-board BDM interface with USB connection. Board is also powered in this way.

Just finishing my first design with the QG8; received some samples a few weeks back, seems to go very smooth. Nice device to work with.

Board are on stock and orderable at Avnet Silica in Europe.

Regards,

 

Cheesehead

0 Kudos
Reply

1,667 Views
FC
Contributor III

 


 


Cheesehead wrote:

Hello FC,

Yes, I have the QG8 Demoboard for some time; had no issues with this after updating my CodeWarrior for the support of the device. Comes complete with Codewarrior and an on-board BDM interface with USB connection. Board is also powered in this way.

Just finishing my first design with the QG8; received some samples a few weeks back, seems to go very smooth. Nice device to work with.

Board are on stock and orderable at Avnet Silica in Europe.

Regards,

 

Cheesehead



 

I recieved the board, but cannot connect to it from CodeWarrior.  The debugger locks up.  The driver is installed fine and the demo program is running.

Any ideas?

0 Kudos
Reply

1,667 Views
okasional
Contributor I
Can anyone explain how to use CW to read the flash memory on this board?
0 Kudos
Reply

1,667 Views
jazz
Contributor I
Hi,

Is the QG8 microcontrollers hooked to the DEMO kit? May I just program using the DEMO board and use the microcontroller alone in another design?

Thanks!
0 Kudos
Reply

1,667 Views
peg
Senior Contributor IV

Hi Jazz,

Not entirely sure what you mean by hooked. Yes of course you can pull out the chip and use it in another board. Also there has been other discussions on using the QG8 demo board as a "cheaper than P&E" BDM adapter for use with QG8's and others. That is, using the demo board to facilitate programming and debugging other chips mounted in circuit on other boards with a BDM header fitted.

BR Peg

Message Edited by peg on 03-18-200610:27 AM

0 Kudos
Reply

1,667 Views
wade
Contributor I


FC wrote:
Has anyone used the new MC9S08QG8 demo board ?






Got one as soon as I could. I'd never used the BDM interface before and I'm hooked now. The board is well worth the money as a BDM alone
Wade H
0 Kudos
Reply