Hello All,
I need a clarification related to Bus Off detection, dependency with CAN transceiver.
Transceiver : TJA1043
Controller: Renesas RH850
During my testing on the Bus Off detection, I have observed that in the
following scenarios, Bus Off detection is not happening.
- CAN_H is connected and CAN_L is opened
- CAN_H is opened (not connected) and CAN_L is connected.
I would like to understand is there any limitation with the TJA1043 in
detecting the above scenario ?
Thanks,
Shan
tja1043
解決済! 解決策の投稿を見る。
Hello All,
As per the clarification got from NXP, The CAN controller can able to read back its own sent messages even though the bus line is open.
Hence, there won't be a chance of transmit error count, only the receive error count will get increased due to no acknowledgement. So, "Bus Off" will not happen when CANH or CANL is disconnected from the network.
Thanks,
Shan
Hello All,
I have found a FMEA matrix table from the Application hints document for TJA1043.
In that it says that if CANH or CANL is open Transmission not possible.
I have confusion, if controller tries to transmits the messages in this scenario,(i.e. CANH or CANL open), will it detect the transmit error or the No acknowledgement error.
I hope there will be a no acknowledgement error. Because if CANH or CANL is open still Controller can able to read backs the information what it has sent successfully.
Is it correct? can someone please clear my confusion.
Thanks
Shan
Hello All,
As per the clarification got from NXP, The CAN controller can able to read back its own sent messages even though the bus line is open.
Hence, there won't be a chance of transmit error count, only the receive error count will get increased due to no acknowledgement. So, "Bus Off" will not happen when CANH or CANL is disconnected from the network.
Thanks,
Shan