Support Required for Migration from MCHC11F1CFNE3 to MC68HC11F1CFN3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support Required for Migration from MCHC11F1CFNE3 to MC68HC11F1CFN3

1,618 Views
AVON
Contributor II

I am in the process of migrating from the MCHC11F1CFNE3 microcontroller to the MC68HC11F1CFN3. I would like assistance in understanding the key differences between these two MCUs and any necessary modifications required for a smooth transition. Specifically, I need guidance on hardware and software compatibility, register differences, and any potential issues that might arise during the migration.

Please provide relevant documentation, migration guidelines, or any recommendations to ensure a successful migration process.

Tags (2)
0 Kudos
Reply
5 Replies

1,540 Views
AVON
Contributor II

Dear Pablo Ramos,

 

We replaced MCHC11F1CFNE3 with MC68HC11F1CFN3, but the system stopped working.

When we use MCHC11F1CFNE3 (we have 2 units), everything works fine.

Could you clarify the difference between these two ICs? We assumed they were the same.

0 Kudos
Reply

1,445 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi,

I apologize for delayed response

Since both MCUs are at end of life or discontinued the information is limited.

We do not recommend the use of part number no RoHC compliance .

I will need to ask you to please contact your distributor for further information on MC68HC11F1CFN3 part.

If you are considering a replacement, just take in consideration that the latest 8 bits MCUs we have had different architecture, this meaning that any replacement will be required HW and SW changes.

In the 8-bit S08 MCU portfolio I can recommend you take a look to the S08PB and S08PL series.

0 Kudos
Reply

1,591 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi, 

The original part was the MC68HC11F1CFN3. When the part changed to lead-free, the new family was MCHC11, without the '68'. For easy identification, we added an 'E' to indicate lead-free in many of the legacy Freescale parts.

This is why, if you go to the product page and open the datasheet you can find the MC68HC11F1CFN3 part number.

Best Regards

Pablo

0 Kudos
Reply

1,457 Views
AVON
Contributor II

Hi Pablo,

I’m still waiting for your response regarding the compatibility between MC68HC11F1CFN3 and MCHC11F1CFNE3. Please confirm if these two are interchangeable.

Our production is currently on hold due to the unavailability of the MCU.

If MC68HC11F1CFN3 is not compatible with MCHC11F1CFNE3, I will need to proceed with selecting an alternative MCU, as NXP has not been able to provide timely technical support.

0 Kudos
Reply

1,578 Views
AVON
Contributor II

Dear Pablo,

Thank you for your response and clarification regarding the part number differences. However, I am facing an issue where my system works fine with MCHC11F1CFNE3, but when I use MC68HC11F1CFN3, it does not function correctly.

Could you please help me understand why this might be happening? Are there any hardware or software differences that could be causing this issue?

0 Kudos
Reply