Solder 1321x, 13213 71-pin LGA package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Solder 1321x, 13213 71-pin LGA package

2,204件の閲覧回数
sli267
Contributor I

I am encountering great problems with soldering MC1321x -the LGA 71-pin package.

The prototype board I made is unmasked... I am hearing a lot of 'no's from commercial PCB prototype companies when I asked them to solder the MC13213 chip onto my board.

 

has anyone successfuly soldered a MC1321x onto an unmasked board? If so... how did you do it??!!

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,513件の閲覧回数
kook
Contributor I

I think you need the following:

 

- activated carbon mask;

- protective glasses;

- latex gloves;

- two syringes;

- a cotton swab;

- a little brush;

- isopropyl alcohol;

- kapton tape;

- an hot plate, something like this http://uk.farnell.com/productimages/farnell/standard/401501006-30.jpg
- tin paste;

- microscope (10X at least);

- directional light for microscope;

- liquid flux;

- a wood block;

- flux cleaner.

 

You have to solder the device in a non conventional manner, because the classical soldering pen is completely useless in this case.

The process  is quite simple, but patience and careful are essential. The entire process can take even hours, depending on the device to be soldered, and must be performed BEFORE the board component mounting.

 

Caution: the following procedure can be dangerous for health, so remember to wear mask, glasses and gloves from begin to the end!!!! All the following steps need to be done near an open window or under an extractor fan.

 

First of all, either the board and the device must be extremely well cleaned with isopropyl alcohol, because dirt and grease can compromise the job.

Fill the first syringe with the liquid flux, remove the needle from the second syringe and place the cotton swab in its back, to make it easier to manage.

Place the device on the board in the correct position, mark its position with the kapton tape and remove the device. Precision in this step is crucial, because it will make easier to hold in place the device during soldering process.

Now you can turn on the hot plate and set it to about 210 - 220°C (392 - 410°F). It will take a little, so you can work on the board. Place the board under the microscope and,with the aid of the syringe needle, spread a thin layer of tin paste on every pin to be soldered. From now unti the final washing of the board, the process is done under the microscope. Once every pad has been covered, the board can be placed on the hot plate to begin the soldering process. As soon the tin paste begins to melt, use the first syringe to apply a thin layer of liquid flux all over the pads and place the device on the board within the kapton marks. Hold and press it in place with the back of the cotton swab for about 3 seconds then remove the board from the plate and place it on the wood block to let it cool down slowly, always pressing and holding down the device with the cotton swab. After about a minute, release the pressure and wash the board while it's still warm with the flux cleaner and the little brush. Wash again the board using isopropyl alcohol and check for problems under the microscope.

 

If all the steps has been done correctly, you now have a completely soldered LGA package to a board.

You can now begin the normal copmponent mounting process.

 

Greetings from Italy,

Valentino

 

P.S.: I'm sorry for my poor english :smileyhappy:

0 件の賞賛
返信

1,513件の閲覧回数
liamj86
Contributor I

Thank you very much for this excellent method!

It will be very helpfull to solder difficult cms packaged component like the MC1321x.

 

Regards,

Liam

0 件の賞賛
返信

1,513件の閲覧回数
liamj86
Contributor I

Hello,

 

I am in exactly the same case, and I wanted to know if you havefound a solution since? Did you do it by hand? Did you find a socket?

 

Thanks!

 

 

0 件の賞賛
返信

1,513件の閲覧回数
sli267
Contributor I

I understand how frustrating it must be.

In the end, I found a circuit designer in the community who soldered it on for me. I think he did it in an oven. Not exactualy sure how he did it... Try calling up electronic shops in your area and see if they know anyone..

0 件の賞賛
返信

1,513件の閲覧回数
liamj86
Contributor I

Thanks!

I think I'll do that, but I continue looking for a mecanical solution.

 

Regards

0 件の賞賛
返信