Single wire porgramming for SG4/SG8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Single wire porgramming for SG4/SG8

1,604 次查看
Deepak1
Contributor IV
Dear Sir,
         I am using SG4/SG8 device.For flash programming i have to use pins /RESET,BKGD,VDD,VSS. Insted of all these i want to use only one pin for flash programming. Is it possible. If so,How..??
 
Kind Regards,
Deepak 
标签 (1)
0 项奖励
回复
2 回复数

742 次查看
celsoken
Contributor V
Dear Deepak,

I am currently using one-wire (plus GND). In my schematics I use 0.1A PPTCs in BKGD and GND lines to avoid damage due to target short-circuits.

You must guarantee  that when the unit powers up the BKGD is kept at 0V. I also suggest that you use a pull-up in the reset and BKGD lines.

If you need automatic pwr-up control, you could use the /RST n-msecs signal generated by Multilink (I assumed you are using ML) to set a flip-flop responsible for engaging the target power.

Good luck,

Celso

0 项奖励
回复

742 次查看
Ake
Contributor III
Hi,
The /RESET signal, is not necessary. You can apply power to the VDD instead. The VSS is ground that is always needed. The last one the BKGND pin is one you need.
 
Regards,
Ake
 
0 项奖励
回复