For production I need secure flash. When in CreateImage.exe is set Secure Device then processor is secured but it is not able re-program again with image where is used EraseModule.? I don´t know why? The CyclonePro stop in security flag.
The image is with commands:
CM
SS
EM ;Erase Module
PM ;Program
PT ;Trim
VM ;verify
SD ;secure
In Metrowerks or in CyclonePro_ProgHcs08.exe is able Erase Module. But why not in Cyclone Image?
Next: When I set NVBACKKEY0-7 for key and KEYEN = 1. Where I can set BACKKEY in programmer for reading code? I can secure but never read? In HC08 was not problem in HCS08 ???