S08QG8 fails to run or debug with VDD under 2.0V.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08QG8 fails to run or debug with VDD under 2.0V.

ソリューションへジャンプ
1,840件の閲覧回数
w_tension
Contributor III

My power source is a digital DC supplier. Things work fine when voltage is equal or above 2.0V. 

Then I turn down the voltage. It always displays this window, though I did re-powered. The chip is S08QG8.

TIM截图20171225173138.png

TIM截图20171225173521.png

タグ(2)
0 件の賞賛
返信
1 解決策
1,602件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Yes, the situation is as what you observed. Although the S08QG8 device is able to operate at 1.8V, it is required to pass the minimum level of Low Voltage Detect circuitry. When the device is powered on, the VDD ramp increases from 0V to VDD, but it is required passing the VLVDL threshold in order to allow the MCU to start operating. Thus, it is required to powering on the device with a VDD value greater than 1.9V (typical) in order to release the reset of LVD.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,603件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Yes, the situation is as what you observed. Although the S08QG8 device is able to operate at 1.8V, it is required to pass the minimum level of Low Voltage Detect circuitry. When the device is powered on, the VDD ramp increases from 0V to VDD, but it is required passing the VLVDL threshold in order to allow the MCU to start operating. Thus, it is required to powering on the device with a VDD value greater than 1.9V (typical) in order to release the reset of LVD.

0 件の賞賛
返信
1,602件の閲覧回数
w_tension
Contributor III

RM says MCU is in reset before rising over  typically 1.9V, How can I use it at 1.8V?

TIM截图20171225201642.png

0 件の賞賛
返信