S08QE8 with External Oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08QE8 with External Oscillator

1,083件の閲覧回数
MatthewScott_DE
Contributor II

I am designing with the 16 pin S08QE8 and plan to use an external oscillator (not a crystal or resonator).  Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging or is there another setup that should be used?

 

Thank you very much for your time

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

945件の閲覧回数
MatthewScott_DE
Contributor II

Thank you both very much

0 件の賞賛
返信

945件の閲覧回数
rocco
Senior Contributor II

Hi Matthew Scott,

 

Welcome to the forum.


Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging?

Yes.

 

0 件の賞賛
返信

945件の閲覧回数
bigmac
Specialist III

Hello,

 

An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.

 

Regards,

Mac

 

0 件の賞賛
返信

945件の閲覧回数
rocco
Senior Contributor II

bigmac wrote:

An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.


Good point. You do not need to "leave it hanging". You can do something useful with it.

0 件の賞賛
返信