S08PT60-EVK RGB program

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S08PT60-EVK RGB program

481 次查看
transistor_vaglienty
Contributor I

I need the original program that was include into the board,

1 回复

446 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @transistor_vaglienty,

The only software currently available for the S08PT60 is the example code provided in CodeWarrior v11.1 and the AN4690SW, which is available in the documentation section of the S08PT.

S08PT|8-bit 5V Full-featured MCU with EEPROM and TSI | NXP Semiconductors

Best Regards,
Pablo

0 项奖励
回复