Re: MC9S08GT32A processor in a auto satellite tracking system for motorhome

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: MC9S08GT32A processor in a auto satellite tracking system for motorhome

1,693 次查看
andrewstancliff
Contributor I

Just a thought before I remove the user interface from the RV.

Do you think is possible there may be data contained on the user interface with all the control switch sand display, it is quite a major process removing this so thought I would ask prior to the removal operation.

 

regards

andrew

标签 (1)
0 项奖励
回复
6 回复数

1,489 次查看
andrewstancliff
Contributor I

Can any nice person out there find where in the attached decoded file the frequencies for the 16 stored frequencies that i need to change

Thanks in advance

0 项奖励
回复

1,489 次查看
egoodii
Senior Contributor III

I'm afraid the code in Astra24.s19 doesn't 'do' anything.  It has a basic 'startup' routine to clear some RAM, which turns out to be ONE byte, and it has a routine at 0x800E that is prepared to 'call' a list of functions from a pointer table, but that list is empty and the count zero.  After that, it just sets a flag in RAM and spins in a dead-end loop clearing the watchdog.  It accesses NO peripherals, sets no I/O of any kind.

And I can't make heads nor tails of Astra23-s19 - Shortcut List.txt --- what process made that and what do you hope it represents?

SUB8000: PSHH;Fetch next byte, increment pointer@0x178
PSHX
LDHX5,SP
LDA,X
AIX#1
STHX5,SP
PULX
PULH
RTS

;

SUB800E: AIS#2;Call a list of routines pointed to from 80C9
LDHXC0X80C1  ;=0    <-count of said list entries
AIX#-1
STHX1,SP ;0xFFFF->0x176
BRALB8035
LB801A:LDA1,X
LSLA
LDX,X
ROLX
ADDC0X80C4  ;=0x80C9
PSHA
TXA
ADCC0X80C3
PSHA
PULH
PULX
LDHX,X
JSR,X
TSX
TST1,X
BNELB8033
DEC,X
LB8033:DEC1,X
LB8035:TSX ;Already negative, do nothing
TST,X
BGELB801A
AIS#2
RTS

;

SUB803C: AIS#-4
LDAC0X80BC  ;=1
INCA
TSX
STA1,X ;2->0x17B
LDAC0X80BB  ;=0
INCA
STA,X ;1->0x17A
LDHXC0X80BD  ;=0x80C5
BRALB806E
LP804F:PSHX
PSHH
LDA,X ;Fectched from 0x80C5
PSHA
LDA2,X
INCA
STA6,SP ;1->0x17C
LDA3,X ;0x01
LDX1,X ;0x80
PULH ; HX = 0x0080
INCA ;A=2
BRALB8064
LB8061:CLR,X       ;Clears one RAM, starting at 0x80
AIX#1
LB8064:DBNZALB8061
DBNZ5,SP,LB8061 ;Dec 0x17C
PULH
PULX
AIX#4 ;0x80C5 goes to 0x80C9
LB806E:DBNZ2,SP,LB804F ;Dec 0x17B
DBNZ1,SP,LB804F ;Dec 0x17A
LDHXc0X80BF  ;=0x80DB
PSHX
PSHH
LB807B:BSRSUB8000 ;Nets 0x00
TAX
INCA
STA3,SP ;1->0x17A
JSRSUB8000 ;Nets 0x00
INCA
STA4,SP ;1->0x17B
DECA
BNELB808F
CBEQX#0x00,LB80AA ;So THIS path is taken
JSRSUB8000
PSHA
PULH
JSRSUB8000
TAX
BRALB80A0
LB809A:JSRSUB8000
STA,X
AIX#1
LB80A0:DBNZ4,SP,LB809A
DBNZ3,SP,LB809A
BRALB807B
LB80AA:AIS#2
JSRSUB800E
AIS#4
RTS

ENTRY:LDHX#0x0180
TXS
BSRSUB803C
JMPLB80CD;Flag 'end' and die there

C0X80BB DB  0x00

C0X80BC DB  0x01

C0X80BDDW  0x80C5

C0X80BFDW  0x80DB
C0X80C1DW  0x0000
C0X80C3DB  0X80
C0X80C4DB  0xC9

C0X80C9: DW 0

DW  0
LB80CD:CLI
JSRSUB80D6
LB80D1:STA0x1800;Just sit here and keep the watchdog happy
BRALB80D1
SUB80D6: MOV#0x01,0x80;Set 'done' Flag in that one RAM byte
NOP
RTS
C0x80DBDW  0
0 项奖励
回复

1,489 次查看
andrewstancliff
Contributor I

The list.txt file comes from code warrior decoder.exe and is "allegedly" the decoded s19 file for hc08 and is a MASM Listing (.lst) type file that opens in Visual C++ by default. I think the extension was changed on upload to site.

I was hoping it may contain comments or something useful, there must be something somewhere hiding away as I know the manufacturer uses the cyclone pro to program and update the system and the other chip on the board which is a Altera cyclone 2 can not be read or programmed via BDM as far as I know as I had to read that with a USB Blaster

I did wonder if there may be something with in the LCD control panel that stores data, however that is a major task removing it.

It has come to the stage after spending £150 on the USB blaster and £450 on the cyclone pro I start to think is it worth for a £1500 system lol!

But I really do appreciate all your help.

Regards

Andrew Stancliffe

0 项奖励
回复

1,489 次查看
egoodii
Senior Contributor III

What I find in there is the first 20% looks more like a hex-dump of the attached PC, what with directory paths and all, like: C:\Users\Andrew\My Documents.  The disassembly seems to be of that same space, and only covers thru 0x3522 (which is below the S08GT32A flash space, which starts at 0x8000).

0 项奖励
回复

1,489 次查看
andrewstancliff
Contributor I

It is all very strange indeed.

One thing I just pondered on was the endless loop you mentioned in an earlier post, The dish opens up then blind scans the sky for a max of 300 seconds could this be this? if within the 300 seconds it receives a signal from the correct satellite it then locks onto that and the search ends. I presume the signal to stop would come from the on-board receiver

I have taken the step of removing the control panel an attach a picture of it from what I can see the Texas71576B is what sends a signal for positional motors to operate. I have done a google for the PCB hmi 0370.002.b but it returns a empty search return ......well it was a long shotIMG_0798.JPG.jpg

0 项奖励
回复

1,489 次查看
egoodii
Senior Contributor III

The code I have managed to disassemble interacts with NO I/O pins, no internal peripheral devices in any way, and as such cannot be doing ANYTHING within you circuit as programmed.  I can only assume what we have is a 'placeholder' for more complex functions that COULD be incorporated.  The 'loop' I mentioned is just where that little bit of code 'goes to die' when it has done the little bit of nothing it does.  Anything that looks like any kind of 'real activity' is coming from somewhere else entirely.

0 项奖励
回复