QG8/GT8-SCL locked to low by slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QG8/GT8-SCL locked to low by slave

1,017件の閲覧回数
icarus31
Contributor III

Hi,

 

I have an IIC master and slave system. The master board uses a NXP LPC2103 chip and the slave board uses a freescale QG8 or GT8 (the code is the same)

 

Very rarely (but it happens), the IIC stopped to work between the master and slave. What I noticed is the slave is locking down the SCL port to low. The SDA is low too, BUT it is released once I disconnect the master (there is a harnesse between them).

 

Right now, I have a timer that is reset each time I receive a IIC communication (by interrupt). If the timer is exceeded, I have a determine there is an IIC failure. I noticed that I am not doing anything with the SCL, SDA or even the IIC itself. Should I? If so, what should I do? Does reading again the IICD can fix the problem?

 

I am a bit lost, because this is something that can take VERY long time to happen (if it does).

 

It is possible the real problem starts with the master board, but I still want to protect my slave board in case it happens again.

 

Any thoughts or suggestions?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

886件の閲覧回数
icarus31
Contributor III

I found, in the forum this one:

 

https://community.freescale.com/message/29205#29205

 

This is what I will try and see if it works (Disable and Re-enable the port)

0 件の賞賛
返信