Hi,
The QE128 is running from an external 32kHz crystal with a bus speed of 1.245MHz. I can't seem to get the real-time counter to work if the ERCLK is selected as the source. These are the register settings:
ICSC1 = %10000000
ICSC2 = %11011111
ICSSC = %00100000
RTCSC = %10110001
The RTC interrupt is called as expected if the LPO is selected or the IRCLK is enabled and selected as the source.
What am I missing?
Thanks,
Andrew
已解决! 转到解答。
I found the stupid error. I switched to the external oscillator before enabling it. :smileysilly: