Hello,
I have read your message, but I am afraid I cannot help you without more information.
I would like to know the following:
 
1) Do you have a development system where you can program and run the HC908LJ12?
And do have it attached when the problems appear?
 
2) Have you tried to write a simple program that sets up an I/O port and wiggle with a pin?
 
3) Does this problem appear after you have developed a product, burned an HC908LJ12, and tried to run it on its own?
 
4) That the output voltage on two I/Os seem to quite low could indicate some trouble with the Vdd.
What voltage have you got there?
 
Well, I can't promise that I can help you. But at least I could try.
 
Regards,
Ake