Problem with AN3927 using JM60 in windows 10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with AN3927 using JM60 in windows 10

1,444 次查看
eduardo1
Contributor II

Hello,

i'm trying to use AN3927 for a msd booloader on JM60, but, always there's a error message "Device cannot start(code 10)" in device manager. I'm using Wireshark to see the communication between host and device(JM60) and i saw a problem with "Get Max Lun Response". The device don't send the correct information and the problem i called happens, but, in windows Xp it works normally. what change in code i need to do for solve the max Lun packet.

pastedImage_1.png

标签 (1)
0 项奖励
回复
1 回复

1,401 次查看
eduardo1
Contributor II

I solved the malformed packet problem with max get lun, but, i saw the scsi commands routines doesn't works. There isn't return with Inquiry command routine. How the microcontroller knows the variable who send the information to the host? I need to pointer to this variable and i don't know which is.

0 项奖励
回复