Pb on DEMO908QB8 with CW5.0 when flashing the HC908QB8 : error 48

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pb on DEMO908QB8 with CW5.0 when flashing the HC908QB8 : error 48

3,586 次查看
R_yM_n29
Contributor I

Hello,

After, i contacted the assistance, i try to obtain an answer on this forum about my problem.

 

I will need your assistance concerning a project in progress on the use of a chart DEMO908QB8.

It is that I often have a problem when I flash his memory, which seems well to proceed, until the moment when, I received the following message:

"CPROG08SZ Programmer"

Error 48 (about the memory protection)

I do not find anything on this subject in all the help files provided with code warrior (version 5).

I does not include/understand, because I had notched the opposite before the launching of the operation, while asking the utility not to protect the memory, but to authorize any obliteration at the time of the writing.

Could you guide me to leave this dead end?

Thank you in advance.

标签 (1)
0 项奖励
回复
5 回复数

1,164 次查看
peg
Senior Contributor IV

Hi Rayman,

As far as I can tell error 48 is "Error contacting target". There are several other messages for problems between PC and your MON08 interface. So the problem seems to be more associated with the MON08 to MCU comms.

What do you have for a clock source? (Crystal?)

If its internal maybe the problem is the erased OSCTRIM value!

Regards David

 

0 项奖励
回复

1,164 次查看
R_yM_n29
Contributor I
Hello,

> > What do you have for a clock source? (Crystal?)


I use an external oscillator (function generator) at 9,8304 MHz, because internal oscillator at 4MHz does'nt work with 9600 and 19200bauds Sci.

This fact OSCTRIM thus does not seem concerned.

Thank you for your assistance!

R.N.
0 项奖励
回复

1,164 次查看
eckhard
Contributor V
Hello,

i have the same problem. The programmer works for other HC08 devices but using the QB8 I get Error 48. Sometimes I can program it once and the I have to wait a few hours to program it again. Else I allways get the error 48. Never managed to get a whole programming and debugging cycle done.

Eckhard
0 项奖励
回复

1,164 次查看
rhinoceroshead
Contributor I
This is drawing at straws here, but I had problems similar to that on the GP32 - where it would work and then 10 minutes later the Flash would not program anymore, then an hour later and it would start working again.  I had the Vtst on the IRQ pin set at 7.5 volts.  When I raised it to 8 volts I never had the problem again.  I don't remember what error message I was getting, but I remember that the problem was intermittent and frustrating.  I don't know anything about this demo board - does it require you to apply Vtst - or does it derive it from the serial driver's charge pump?  You might try measuring the Vtst voltage to make sure it is towards the middle of the allowed range.  Just a thought.
0 项奖励
回复

1,164 次查看
eckhard
Contributor V

Hello,

I have a 8.2 V Zened diode on Vvtst. and a RC on the reset pin so Vtst should be up right in time and I can measure the 8.2 Volts on the Vtst pin. Tried to connect 9V from the power source and not from the max232 with no success.

 

Eckhard

0 项奖励
回复