PLEASE HELP ME.................connect serial device to 1321x NCB board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PLEASE HELP ME.................connect serial device to 1321x NCB board

1,252 次查看
bitasobhani
Contributor III

Hi all

I want to connect an optical port to 1321x NCB board.  Both have female RS232 ports. How should be the wiring for connecting this two female serial devices?

Thanks 

标签 (1)
0 项奖励
回复
1 回复

657 次查看
bigmac
Specialist III

Hello,

 

I assume that you are referring to DB9 (9-pin) female connectors on both boards.  If so, it is possible that both boards are configured as "data communications equipment" (DCE).

 

However, the use of a standard 9-way through lead assumes that the DCE device is connected to a "data terminal equipment" (DTE).  A computer serial port is normally configured as a DTE.

 

For a DCE to communicate with another DCE (or for two DTEs to communicate), a special lead or adaptor is necessary.  This is called a "null modem".  You might purchase a null modem adaptor, or alternatively make your own null modem lead.

 

In the latter case, the data connections will need to be swapped, as a minimum.  If hardware handshaking is implemented, other swapped connections may also need to be present.

 

End 1:          End 2

TXD ----------- RXD

RXD ----------- TXD

RTS ----------- CTS

CTS ----------- RTS

DTR ----------- DSR

DSR ----------- DTR

GND ----------- GND

DCD No connection

RI  No connection 

 

Regards,

Mac

 

0 项奖励
回复