Dear All,
I have two questions.
(1)tSPI_EN value is ??
Which document I can find this value?
I didn't find this value in both ntm88 manual & SPI programming doc.
(2)BACKGROUND mode
How to program sensor in BACKGROUND mode?
I pull low BKGD pin then reset NTM88 pin to enter BACKGROUND mode .
It looks like failed, I can't program NTM88 sensor by external mcu SPI interface.
But, if I pull low BKGD then turn off-> turn on sensor power, it can enter BACKGROUND mode.
What’s the difference? Is that possible to enter into BACKGROUND mode by BKGD low then reset sensor by RSTB ?
Thanks.
解決済! 解決策の投稿を見る。
1:tSPI_EN parameter value showed in datasheet page13.
2: If the BKGD/PTA4 pin is held low when the device comes out of a
power-on-reset (POR), the device switches into the ACTIVE BACKGROUND
DEBUG mode (BDM).
1:tSPI_EN parameter value showed in datasheet page13.
2: If the BKGD/PTA4 pin is held low when the device comes out of a
power-on-reset (POR), the device switches into the ACTIVE BACKGROUND
DEBUG mode (BDM).