NTM88 SPI tSPI_EN time & BKGD background mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTM88 SPI tSPI_EN time & BKGD background mode

ソリューションへジャンプ
1,476件の閲覧回数
Thomas_2022
Contributor I

Dear All,

 

I have two questions.

(1)tSPI_EN value is ??

Which document I can find this value?

I didn't find this value in both ntm88 manual & SPI programming doc.

(2)BACKGROUND mode

How to program sensor in BACKGROUND mode?

I pull low BKGD pin then  reset NTM88 pin to enter BACKGROUND mode .

It looks like failed, I can't program NTM88 sensor by external mcu SPI interface. 

 

But, if I pull low BKGD then turn off-> turn on sensor power, it can enter BACKGROUND mode.

What’s the difference? Is that possible to enter into BACKGROUND mode by BKGD low then reset sensor by RSTB ?

Thanks.

 

0 件の賞賛
返信
1 解決策
1,410件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1:tSPI_EN parameter value showed in datasheet page13.

2: If the BKGD/PTA4 pin is held low when the device comes out of a
power-on-reset (POR), the device switches into the ACTIVE BACKGROUND
DEBUG mode (BDM). 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,411件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1:tSPI_EN parameter value showed in datasheet page13.

2: If the BKGD/PTA4 pin is held low when the device comes out of a
power-on-reset (POR), the device switches into the ACTIVE BACKGROUND
DEBUG mode (BDM). 

0 件の賞賛
返信