MQ8CE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQ8CE

2,282 次查看
wojciechfranczu
Contributor I

Dear Sirs,

Is it possible to get any information from you(datasheet, application note) about IC  MQ8CE?  It is IC with Freescale logo and  QFN16 package. I would appreciate any help from you. Is it programmable microprocessor?  I want to repair very important for me equipment and have no idea if after I buy the new one it will work (without application and program I have no chance so no need to buy).  This IC is put between ST Bluetooth module and main microprocessor.

Thank you in advance for any help.

Your faithfully,

Wojciech Franczuk

Poland

+48 790 270 487

标签 (1)
0 项奖励
回复
2 回复数

1,711 次查看
david_diaz
NXP Employee
NXP Employee

Hello Wojciech,

I am glad to help.

The device you are speaking is the MC9S08QG8 MCU.

The S08QG Family of microcontrollers provide a wide variety of serial interfaces and peripherals, normally found in higher-end devices, all in a small package. Featuring low-power S08 8-bit architecture, S08QG devices are a perfect fit for battery-powered devices.

You may find useful information as the datasheet and application notes (Documentation tab) at the following link:

8-bit Small Package QG MCUs|NXP

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 项奖励
回复

1,711 次查看
wojciechfranczu
Contributor I

Hello David,

Thank you very much for your answer. It is exactly what I was asking

for. Now I know haw to check the circuit and read the memory.

Thank you again,

Regards,

Wojciech Franczuk

W dniu 2016-06-08 o 16:39, david_diaz pisze:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

MQ8CE

reply from David Diaz Marin

<https://community.nxp.com/people/david_diaz?et=watches.email.thread>

in /8-bit Microcontrollers/ - View the full discussion

<https://community.nxp.com/message/663313?et=watches.email.thread#comment-663313>

>

0 项奖励
回复