MCU with display driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCU with display driver

1,781 次查看
hasaur
Contributor II

Hello.

I have a display like this one (http://www.lextronic.fr/P1614-afficheur-tactile-couleur-320-x-240-dpp-ctp3224.html) and I would like to know if there is a 8bits MCU with a driver to control it.

Thank you in advance.

标签 (1)
0 项奖励
回复
3 回复数

1,223 次查看
bigmac
Specialist III

Hello,

 

It would appear that the display device has several interface options available, including serial port (SCI), IIC (often known as I2C), and SPI (slave?).  Most Freescale MCUs incorporate the hardware for one or more of these communication methods.  Many devices will incorporate all three peripheral modules.  SPI is likely to provide the fastest communications.

 

A further USB option for the display is really intended for PC usage, rather than for a MCU application.

 

Regards,

Mac

 

0 项奖励
回复

1,223 次查看
hasaur
Contributor II

Thank you very much.

I have a 16bit MCU (MC9S12XEP100) that already has much work to do and I would like to know if I can drive the display with it or if it will become slow (and I'd rather use a 8bit MCU in addition, specially for the display). And if it's better to use a 8bit, which one would be a good choice (because there is too many 8-bits that incorporate SPI module) ?

 

Thank you for your help. 

0 项奖励
回复

1,223 次查看
bigmac
Specialist III

Hello,

 

Since the display device you have chosen appears to have been designed to simplify the interface between the display and a MCU, I would doubt the neccessity for an additional intervening processor.  You would still require a communications interface between the 12XEP100 and the display processor, so nothing to gain here.

 

So it will depend on the amount of data to be sent to the display processor, versus the amount of data required by the display itself.  There would need to be a massive disparity to justify an additional processor.  Maybe if your application required high resolution graphics with rapid animation.

 

Regards,

Mac

 

0 项奖励
回复