MCU in MC13213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU in MC13213

1,343件の閲覧回数
Thomas_H
Contributor I
Hello,

please could anyone tell me which controller is in the MC13213 RF transceiver? It should be an MC9S08GB60 or a MC9SGT60.

regards
Thomas
ラベル(1)
0 件の賞賛
返信
1 返信

726件の閲覧回数
peg
Senior Contributor IV
Hello and welcome to the forums Thomas,

The chip inside a GB60 and a GT60 is exactly the same.
The are all mask xL31R (x = 1 to 4)
The GT simply has less pads bonded out to pins.
The MC13213 does not have all pins bonded out either and so is closer to a GT.
You can still use the higher timer channels and such, you just don't have the channel pins etc.

With the A versions of the GT they have actually cut down the die to more closely tie in with what is actually bonded out.
But I believe the Zigbee stuff still uses the old GB/GT (non-A)

0 件の賞賛
返信