MC9S08SH8:I can enter in Stop3 mode but not in Stop2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08SH8:I can enter in Stop3 mode but not in Stop2

Jump to solution
1,343 Views
diegocolombo
Contributor IV

Kind support and community users

 

i'm evaluating MC9S08SH8 power consumption and behaviours in Stop3 and Stop2 modes.

 

Stop3 mode looks running,when entered the current consumption of my circuit(uC plus some low power peripherals) drops from 9 mA to 45 uA.

This does not happens launching Stop2.The  current consumption remains in the mA range

I am using Processor Expert to select the mode,the bit PPDC is write once,and i verify that PPDC=1 before running the "STOP" instruction,The other bits are conformed to table 3-1 of the datasheet .

 

What else should i check?

 

Thanks

 

Diego

Labels (1)
0 Kudos
Reply
1 Solution
1,058 Views
diegocolombo
Contributor IV

It is my fault,sorry

The RESET/IRQ pin was left accidentaly floating.

Measuring the voltage it is low,so the IRQ is asserted,and this wakes the uC immediately or avoid that it enters i STOP2

Resoldering the pullup resistor makes it work correctly

View solution in original post

0 Kudos
Reply
3 Replies
1,059 Views
diegocolombo
Contributor IV

It is my fault,sorry

The RESET/IRQ pin was left accidentaly floating.

Measuring the voltage it is low,so the IRQ is asserted,and this wakes the uC immediately or avoid that it enters i STOP2

Resoldering the pullup resistor makes it work correctly

0 Kudos
Reply
1,058 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Diego

I glad to hear that your problem is solved.

If you have more problem, just let me know

Regards

Vicente Gomez

0 Kudos
Reply
1,058 Views
diegocolombo
Contributor IV

Thanks very much,Vicente

Diego

0 Kudos
Reply