Hallo Community,
I am programming MC9S08QG8 on DEMO9S08QG8 BDM Board. The calculated
frequency / period of time loops corresponds to the measured frequency.
The condition is: To set or delete a port output with bset..., bclear..,
I need 5 clocks instead of 4 as specified in the instruction set list.
With help of BDM interface on demo board I can also program a controller
outside the demo board and it shows the same properties.
if this controller runs separately, its working speed is significantly higher.
I think the already noticed bset, bclear commands run properly outside of BDM
with 4 clocks. For an exact calculation, the bus cycle of the separate controller
would also have to differ slightly from the bus cycle on the BDM board.
The influence of the set / clear commands must be clarified with further measurements,
but maybe someone from the community knows what it is like.
With best Regards
Gerd
.