MC9S08QE32CLC and AD converter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08QE32CLC and AD converter

953 Views
add524
Contributor I

The data sheet says that the input impedance is 5K to 7K. If that impedance is tied to ground inside the micro, then I will need amplifiers. How is that 5K impedance terminated inside the micro?

Labels (1)
0 Kudos
Reply
1 Reply

628 Views
bigmac
Specialist III

Hello,

 

A closer inspection of Fig. 22 within the datasheet shows that Radin represents the series resistance associated with the channel select multiplexer.  This series resistance will interact with the shunt capacitance Cadin.

 

However, the external series resistance (Ras) will have an upper limit mainly determined by pin leakage, and the conversion accuracy required.  For a 12-bit conversion, the upper  limit may be as little as 2k ohm, possibly requiring the use of a buffer amplifier.  The reference manual for the device gives the following formula:

 

Ras < Vddad / (2^N * leakage_current)

 

 

Regards,

Mac

0 Kudos
Reply