MC9S08GT16A internal oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08GT16A internal oscillator

2,981 Views
DanielMorley
Contributor I
I am trying to configure my code to turn on the internal oscillator with out an external one.  The code I am writing comes from the part data sheet.
 
 
 
 ICGC1 = 0b00101000;     
                          
  ICGC2 = 0b00110001;
 
This data sheet also recomends that I assign IGCS1 and IGCS2 with dont care's.  The C compiler will not take don't cares.  So I omitted this step.  Will the code work with out an external register?
 
 
(Alban corrected title: device name)

Message Edited by Alban on 2006-12-11 09:25 PM

Labels (1)
0 Kudos
Reply
5 Replies

1,087 Views
DanielMorley
Contributor I
 MC9S08GT16A is the chip i am using.  I took the code straight from the data sheet. Example three no external oscillator. 
 
 
 
0 Kudos
Reply

1,087 Views
peg
Senior Contributor IV
Hi Daniel,
 
Sorry I misled you before. REFS is only relevant in the external modes.
What you have is correct for FEI mode and gives a buss clock of 5.4MHz.
 
I have an actual product that uses:
ICGC1 00001000
ICGC2 01110000
This gives 19.9954MHz in FEI (trimmed)
 
The only difference is you have x10/2
where I have x18/1
 
Regards
Peg
 
0 Kudos
Reply

1,087 Views
DanielMorley
Contributor I
Can I ommit the ICGS1 & UCGS2, ICGFLTU/L statements out for the oscillator to work.  Or will the code be sufficiant to start up the oscillator.
0 Kudos
Reply

1,087 Views
peg
Senior Contributor IV
Yes you can!
 
Here is my entire ICG initialisation:
 
Code:
*********** Set-up ICG to clock the bus at 19.9954 MHz **********************  LDA NVICGTRIM  ;get calibration value from FLASH  STA ICGTRM   ;set oscillator trim value  MOV #(mMFD2|mMFD1|mMFD0),ICGC2 ;sets MFD divider  MOV #mCLKS0,ICGC1  ;243 kHz -> 19.9954 MHz bus rate  BRCLR LOCK,ICGS1,*  ;loop until FLL locks 

 
Regards
Peg
 
0 Kudos
Reply

1,087 Views
peg
Senior Contributor IV
Hi Daniel,
 
What is a 9SO16A?
 
I thought maybe you meant 9S08GT16A but then your values are fairly obviously wrong.
e.g. REFS is 1 = external clock.
 
So I guess we better figure out which device first.
 
Regards
Peg
 
0 Kudos
Reply