MC9S08GT16A buffering inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S08GT16A buffering inputs

3,236 次查看
Kerms
Contributor I
Hello, I am using an MC9S08GT16A to interface with several 5v sensors. As such I need to buffer the inputs to make them 5v input tolorent.
 
I am looking to use the 74LCX240 to buffer the inputs and was wondering if that was a good choice or if there are others I should use instead.
 
Also can you recommend any bi directional buffers if I wanted to be able to change the direction?
 
Thanks
标签 (1)
0 项奖励
回复
4 回复数

1,185 次查看
Witztronics
Contributor IV
Check out the ADI ADG330x family of parts.

http://www.analog.com/en/prod/0,,767_828_ADG3304%2C00.html

They don't need directional pins.


Message Edited by Witztronics on 2007-12-01 10:45 PM
0 项奖励
回复

1,185 次查看
bigmac
Specialist III
Hello,
 
If the sensors you refer to are the channel outputs from a RC receiver (as described in another post), a satisfactory interface method may be to simply provide a series resistor (say 4k7) for each input.  The intrinsic protection diodes will limit the voltage swing.  Alternatively, you could add an external Schottky diode between each input (anode) and +3V3 (cathode).  The external diode should conduct before the intrinsic diode does.  In both cases, the series resistor will limit current flow.
 
A related method would be to provide a voltage divider to provide 3V3 output for an input of 5V.
 
For any outputs from the MCU, you should first examine whether the external device will operate correctly with a 3V3 swing.
 
Regards,
Mac
 
0 项奖励
回复

1,185 次查看
Technoman64
Contributor III
I have used the following Tiny Logic part to succesfully interface +5v to +3.3v logic. The inputs are 5 volt toleant when operating with a 3.3 volt supply.
 

SN74LVC1G17

 

0 项奖励
回复

1,185 次查看
peg
Senior Contributor IV
Hi Kerms,

That part would seem to be OK.
Have you looked at AN2433
SN74LVC1T45DBV is an example of a bi-directional buffer.

0 项奖励
回复