MC9S08AC ADC power pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08AC ADC power pins

1,639件の閲覧回数
trproc
Contributor I
If the ADC of an S08 MCU with external VDDAD and VSSAD power pins is not used, do the pins need to be left floating or do they need to be connected. If they need to be connected, connected to what? The data sheet does not specify.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

908件の閲覧回数
peg
Senior Contributor IV

Hello,

The ADC power pins should be connected to the processor power pins if unused.

It is often this way when it is used as well, although it would be done with particular attention paid to noise etc from the digital side.

0 件の賞賛
返信

908件の閲覧回数
trproc
Contributor I
Thanks. I appreciate the info.
0 件の賞賛
返信