MC9S08AC ADC power pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08AC ADC power pins

1,587 Views
trproc
Contributor I
If the ADC of an S08 MCU with external VDDAD and VSSAD power pins is not used, do the pins need to be left floating or do they need to be connected. If they need to be connected, connected to what? The data sheet does not specify.
Labels (1)
0 Kudos
Reply
2 Replies

856 Views
peg
Senior Contributor IV

Hello,

The ADC power pins should be connected to the processor power pins if unused.

It is often this way when it is used as well, although it would be done with particular attention paid to noise etc from the digital side.

0 Kudos
Reply

856 Views
trproc
Contributor I
Thanks. I appreciate the info.
0 Kudos
Reply