Hi Jorge,
Do you have an eval board to test the configuration ?
It could be fine to test the configuration (codeWarrior + Multilink).
On my my side it's working fine using Tower kit.
I don't think there is a problem with the Multilink as the 2 leds are switched-on.
The Multulink is detected by CodeWarrior following the Error.png file.
I think there is a problem between the Multilink and the device and this explain the error2.png file.
Most of the time, the message "error2.png" occurs when a wrong power supply is provided on-board or when the Multilink is not correctly connected to the board.
This question is may be more for hardware colleague.
I will move the question to them.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------