MC8S08SH8 buy guide (DIP socket??)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC8S08SH8 buy guide (DIP socket??)

1,082 次查看
pathik
Contributor I

Hi

I want to buy MC8S08SH8 development board from freescale.

this is web link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9S08SH

I am try to find if the 20pin DIP microcontroller is in socket or it is soldered on board??

Because I m planning to use same kit (development board) to programm number of controllers.

 

If anyone have already purchse or if they have idea about kit.

 

Thank you

Pathik

标签 (1)
0 项奖励
回复
3 回复数

885 次查看
bigmac
Specialist III

Hello Pathik, and welcome to the forum.

 

It the photograph shown in the link is currently accurate, it would appear that the MCU is in a SOIC package which is directly soldered to the board.

 

However, the demo board also provides an empty footprint for a 6-pin BDM header, usually available for programming an external board.  For this reason, I suspect it would be feasible to isolate the BDM connection from the on-board device.  You will need to download the schematic for the demo board to verify this aspect.

 

Regards,

Mac

 

0 项奖励
回复

885 次查看
rocco
Senior Contributor II

Hi Pathik and Mac,

 

That page is selling two different boards, but only shows the picture for the 28TSSOP board (SH32). I can't seem to find a picture of the 20PDIP board (SH8).

 

But looking at the manual here:

http://cache.freescale.com/files/microcontrollers/doc/user_guide/DEMO9S08SH8UG.pdf?fpsp=1

 

I suspect it does have a socket. Although it does not state either way (lame), my suspicion is based on the drawing on page 5. First, the silkscreen looks like a socket, and second, the reference designator is "SU1" whereas an unsocketed part would normally be "U1".

 

In any case, you could always replace the chip with a socket. I would go for a ZIF socket if you intend to use it for programming.

 

I could be wrong, I often am, but I never admit it.

0 项奖励
回复

885 次查看
RogerSchaefer
Contributor III

You may want to take a look at my MC9S08SH8 project board.

 

http://www.rasmicro.com/SH8_Board.htm

 

Roger

 

0 项奖励
回复