MC68HC908QB8 & 32.768kHz Crystal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC68HC908QB8 & 32.768kHz Crystal

1,504件の閲覧回数
Kenm
Contributor II
Has anyone any experience using a 32.768Khz Crystal with the 980QB8 processor?
 
The main problem I have is consistency.  I can get the device to oscillate but the capacitors seem to vary significantly between devices.

What Crystal, capacitors, feedback and limit resistors did you use.

--
Alban edit: change subject unit from "Mhz" to "kHz"


Message Edited by Alban on 2007-06-06 10:53 AM
ラベル(1)
0 件の賞賛
返信
1 返信

706件の閲覧回数
bigmac
Specialist III
Hello,
 
Do you mean that you need to vary the capacitor values to achieve oscillation?  If so, it may indicate that you need to reduce the "limit" resistor in series with the crystal.
 
A good starting point for the capacitors would be 22p for each, although to achieve the correct operating frequency may need somewhat different values.  The shunt resistor used for biasing should have a value of at least 1M0, but an even higher value is probably preferred for the low frequency crystal.
 
The series resistor might commence with a value of say 100k, but may need reduction if oscillation is reluctant to start.
 
Be aware that the low frequency crystal may take a second or two to achieve maximum oscillation amplitude.  This will need to be taken into account before switching from the internal oscillator.
 
I don't know the practicality of using such a low frequency crystal for the QB8 device - this will result in a bus frequency of only 8.192 kHz, so operation will be very very slow.  At this frequency, many of the peripherals would not be usable.
 
A better choice may be to use a device containing a PLL or FLL facility to multiply the bus frequency.  The 9S08QG8 might be a possibility.
 
Regards,
Mac
 


Message Edited by bigmac on 2007-06-07 01:15 AM
0 件の賞賛
返信