Let’s dive into the world of microcontrollers and explore the equivalence between the MC68HC and MCHC series.
MC68HC vs. MCHC:
The MC68HC and MCHC series are related families of microcontrollers.
The MC68HC series (also known as the 68HC08 family) includes various 8-bit microcontrollers Receiptify Music
The MCHC series (also known as the HCS08 family) is an evolution of the 68HC08 family, with enhanced features and improved performance.
Specific Models:
For specific models, let’s break it down:
MC68HC908: This refers to a microcontroller from the 68HC08 family.
MCHC908: This likely refers to a microcontroller from the HCS08 family, which is an evolution of the 68HC08 family.
In general, the MCHC908 is an improved version of the MC68HC908, with additional features and enhancements.
Equivalence:
While the exact part numbers you provided (MC68HC908LJ24CPB, MC68HC908LJ24VPB, MC68HC908LJ24MPB) might not have direct equivalents in the MCHC series, the overall architecture and functionality are similar.
If you’re migrating from the MC68HC to the MCHC series, you’ll find that many features and peripherals are compatible.