MC68HC、MCHC Are these two series equivalent?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC68HC、MCHC Are these two series equivalent?

1,514 次查看
anan5188
Contributor I

Hello Engineer,

We want to test several parts and have some issues about it.

MC68HC、MCHC Are these two series equivalent?

For Example,MC68HC908=MCHC908?

I know that S912 and MC9S12 these two models are equivalent. I

f availble,I hope you can help me.I really appreciate your kind assistance!

We can use the below part:

MFR p/n MC68HC908LJ24CPB MFR NXP

Alternative MC68HC908LJ24VPB

Alternative MC68HC908LJ24MPB

Have a sweet day!

0 项奖励
回复
2 回复数

1,115 次查看
ArcticSparks
Contributor I

This is a great breakdown of the similarities and differences between the MC68HC and MCHC series! I appreciate the clear comparison of their evolution and features. It's helpful to know that while the specific part numbers may not have direct equivalents, the overall functionality remains compatible for those looking to migrate. A deeper dive into the key improvements in the MCHC series could be useful for understanding the advantages of upgrading. Great post! Direct2HR

0 项奖励
回复

1,234 次查看
jennie258fitz
Contributor II

Let’s dive into the world of microcontrollers and explore the equivalence between the MC68HC and MCHC series.

MC68HC vs. MCHC:
The MC68HC and MCHC series are related families of microcontrollers.
The MC68HC series (also known as the 68HC08 family) includes various 8-bit microcontrollers Receiptify Music
The MCHC series (also known as the HCS08 family) is an evolution of the 68HC08 family, with enhanced features and improved performance.
Specific Models:
For specific models, let’s break it down:
MC68HC908: This refers to a microcontroller from the 68HC08 family.
MCHC908: This likely refers to a microcontroller from the HCS08 family, which is an evolution of the 68HC08 family.
In general, the MCHC908 is an improved version of the MC68HC908, with additional features and enhancements.
Equivalence:
While the exact part numbers you provided (MC68HC908LJ24CPB, MC68HC908LJ24VPB, MC68HC908LJ24MPB) might not have direct equivalents in the MCHC series, the overall architecture and functionality are similar.
If you’re migrating from the MC68HC to the MCHC series, you’ll find that many features and peripherals are compatible.

0 项奖励
回复