MC68705R3 erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC68705R3 erase

1,328件の閲覧回数
kamilica
Contributor I
Hi I am looking for solution to erase MC68705R3 chip. I have some with window on and they are UV erasable, but majority of them are without.
ラベル(1)
0 件の賞賛
返信
1 返信

684件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora, kamilica.

Presumably the windowed ones are also ceramic with a quartz glass window. This is expensive to manufacture (buy) especially when most devices will only ever be programmed once. Because of this they come up with "OTP" One Time Programmable devices which are the same inside but just molded in plastic. If you need to re-programme these, you throw it away and use a new one.

This is probably what you have. If you don't want what is programmed into them now they are worthless.

 

0 件の賞賛
返信