In this product card write, that MC3PHACVDWE are 8BIT MCU, 8K FLASH OTP. In datasheet i dont found any informations or schematic about MCU. Can you any post schematic or diagram? Or send link with information about MCU include in this part? Very thanks
解決済! 解決策の投稿を見る。
Worfvx, if I'm not crazy the MC3PHAC is a preprogrammed MC68HC908MR8.
Best regards,
Celso
really? Thanks
Maybe i still have the codewarrior project to make it. I'm not sure I can legally publish it.
Regards,
Celso
The MC3PHACVDWE is no longer manufactured. and the internal 8 bit device never was sold as a simple MCU.
Now if you need an 8 bit device for motor control please check the MC9S08MP family
Regards
Vicente
Thanks Vincente, but your answer didn't explain to me if it contains MCU.
Yes It was preprogrammed 8-bit device
with MCU core? Exist diagram of this device, please?
HC08 core, and not, there is not a diagram of this internal device
Sorry
Very thanks for your answer, Vincente
Dear Worfvx,
Sorry for my late answer, the MC3PHAC is really a preprogrammed HC908MR8 device, I´ve got the CW complete project that assembles (yep, .ASM) flawlessly in CW 6.3 running on my WIN10 64-bit (Tks Rod!). There are lots of information on this like An2202, An2988, DRM006 DRM019. Motorola/Freescale really provided excellent documentation.
Check the top of Motor.s listing:
1 1 ;************************************************************************
2 2 ;* *
3 3 ;* Name: Motor.s *
4 4 ;* Project: MC3PHAC Motor Controller *
5 5 ;* Description: top level file *
6 6 ;* Processor: MC68HC908MRx *
7 7 ;* HW: any *
8 8 ;* Revision: 1.1 *
9 9 ;* Date Created: 12/20/1999 *
10 10 ;* Last Revision 02/03/2004 *
11 11 ;* Compiler: CodeWarrior 2.1 *
12 12 ;* Tab Stops: *
13 13 ;* Author: D. L. Wilson *
14 14 ;* Modified by Hayden Fraser *
15 15 ;* Company: Freescale Semiconductor Inc. *
16 16 ;* =================================================================== *
17 17 ;* Copyright (c): FREESCALE Inc.,2004, All rights reserved. *
18 18 ;* =================================================================== *
19 19 ;************************************************************************
Maybe you could still use this code - or parts of it - with the newer S08.
Cheers,
Celso