MC1322x USB dongle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC1322x USB dongle

2,034 Views
Nyarlathotep
Contributor I

Hello everybody,

 

I'm looking for some description of the MC1322x USB dongle pre installed sniffer firmware (or for the source code of it).

I'd like to communicate with the device through virtual COM and I need to know what are the commands available.

Does anybody know where to find such a documentation?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

861 Views
tomlogic
Contributor III

It works with WireShark to capture packets.

 

Install WireShark and the WireShark ZigBee Utility.  You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.

 

Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.  Wireshark will then start displaying and decoding captured packets.

0 Kudos
Reply