MC13213 with an external LNA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC13213 with an external LNA

4,689 次查看
Spell
Contributor I
Hi all,
I need to improve the range coperture of my custom board based on MC13213.
I'm thinking to use an external LNA, like MBC13720, to increase the output power.
Someone have implement a custom board with this kind of device?
I have already asked to Freescale support but they haven't an application note with this device or a reference manual.

best regards, Filippo
标签 (1)
0 项奖励
回复
8 回复数

2,236 次查看
rfquery
Contributor I
Hi all,
Would anyone please share what is the minimum SNR required for detection  and the Noise figure for Freescale MC13213 SRB board. This is needed to calculate (theoretically) by what factor the range can be extended by using an LNA with SRB.
Thank you.
Regards.
0 项奖励
回复

2,236 次查看
muni
Contributor I
Hi,
 
Could you share your schematic which has LNA MBC13720 interfaced with MC13213.
 
Thank you.
 
Regards,
Muni.
0 项奖励
回复

2,236 次查看
rfquery
Contributor I
Hi all,
 Suppose I am using MBC13720 ( a seperate board) with MC13213 board to extend the range( after doing some board rework ) what type of connectors and cables should I use to avoid impedance mismatch?
 
 
0 项奖励
回复

2,236 次查看
Spell
Contributor I
You can use any kind of connector and cable with an impedance of 50ohm at 2.4GHz
0 项奖励
回复

2,236 次查看
ZigBeeficator
NXP Employee
NXP Employee
Hello,
 
In order to use an external LNA with MC13213, please make sure you are in Dual Port Antenna configuration (see MC1321x datasheet), then here is attached a suggested schematic with MBC13720 LNA.
 
Regards
 
Message Edited by t.dowe on 2009-10-27 02:06 PM
0 项奖励
回复

2,236 次查看
muni
Contributor I
Hi friends,
 
If anybody has single antenna schematic for MC13213 (ZigBee modem) with MBC13720(LNA) in tranmit path, please share it with me. Also, I would like to know with this LNA what could be the max range I can achieve.
 
Thanks in advance.
 
Regards,
Muni.
0 项奖励
回复

2,236 次查看
rfquery
Contributor I
Hi,
 Would anyone please share the  calculation of  external matching components values (Inductors and capacitors ) of  MBC13720 for 1.9GHz and 2.4GHz operation.
Thank you.
Regards,
0 项奖励
回复

2,236 次查看
Spell
Contributor I
Hi ZigBeeficator,
thank you for your design.
It's possible to use an external LNA like MBC13720 with a Single Port configuration and use the CT_Bias pin for set the LNA in bypass mode or gain mode?
In this case I don't use the Dual Port Configuration like you have suggested.

best regards, Filippo
0 项奖励
回复