[MC13213-Zigbee] LQI...how is calculated?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MC13213-Zigbee] LQI...how is calculated?

12,733 Views
CecchiSandrone
Contributor II
Hi all,

I'm working on a project regarding relative distance estimation. What we want is a rough distance estimation in indoor places.
I'm reading the Zigbee 2006 standard and they talk about LQI (Link Quality Indicator) but they don't explain deeply how is calculated. Maybe is the value of this field relative to hardware vendor?

Did anyone get some good results using this value for distance estimation?
Can you advise me about articles or publications to consider?


Labels (1)
0 Kudos
Reply
7 Replies

3,564 Views
AmZig
Contributor I
Hi ,
 
According to my little knowledge , you could get more info about LQI from IEEE 802.15.4 . And how its been calculated , if you are using MAC code base then look in file "Data.c ". As , i have used LQI in my project for assosciation between devices. I think from this Data.c file you could get very good idea abt LQI. Here is the code to calculate LQI on Freescale MC13213 boards
oid ConvertLinkQuality(void){
  uint8_t     linkQuality = gpPhyRxData->linkQuality;
  // Recalculate the link quality to conform with other link quality measures
  // Make dynamics of the energy level vary from 0x00-0xff
  if (linkQuality > 190) {
    linkQuality = 190; //190 = -95dBm as floor (translates to 0x00)
  }
  if (linkQuality < 33) {
    linkQuality = 33; //33 = -16.5 dBm as top (saturation)
  }
  linkQuality = 190 - linkQuality; 
  linkQuality = linkQuality + (linkQuality >> 1) + (linkQuality >> 3);
  gpPhyRxData->linkQuality = linkQuality;
}
 
Regards
Amzig
0 Kudos
Reply

3,564 Views
CecchiSandrone
Contributor II
Thanks AmZig, I've found this function. What I want to understand is the relationship between RSS and LQI. If I'm not wrong, ConvertLinkQuality converts RSS (in dBm) to LQi (a value between 00 and FF). In some publications I've found also RSSI (Received Signal Strenght Indicator), are LQI and RSSI the same?
Please clarify this AmZig...thanks!
0 Kudos
Reply

3,564 Views
AmZig
Contributor I
Hello Cecchi,
Good question Cecchi   :smileyhappy: , according to my assumtion , logically they are same . As, LQI is always calculated on the received packet or signal strength , for e.g LQI or MPDU lqi on received packet, and different LQI  of different coordinator in device POS.
0 Kudos
Reply

3,564 Views
CecchiSandrone
Contributor II
So they aren't calculated making statistical analysis. They are only numerical a "transformation" of the RSS.
0 Kudos
Reply

3,564 Views
AmZig
Contributor I
Hello Cecchi,
I didnt understand you clearly. But i would say that the RSS is a parameter for measuring the range or perfomance from one device to another.So , do the LQI when you are trying to do comparison of devices placed different ranges. This is what i have assumed after my project.
 
Regards
AmZig.
0 Kudos
Reply

3,564 Views
bigmac
Specialist III
Hello Cecchi,
 
The attached application note (non-Freescale) may be of interest to you.  It describes location detection issues in some detail.
 
Regards,
Mac
 
Message Edited by t.dowe on 2009-10-27 12:25 PM
0 Kudos
Reply

3,564 Views
CecchiSandrone
Contributor II
I'm a little bit confused guys. I can't understand (if exists :smileyvery-happy:) the difference between LQI contained in Zigbee packets (00 to FF) and RSS (expressed in dBm). Please explain this, thanks.
0 Kudos
Reply