MC13213-SRB Problems linking EVK Switch Demo?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13213-SRB Problems linking EVK Switch Demo?

2,626件の閲覧回数
DARCY_R
Contributor I
I'm trying to compile and link the 802.15.4 EVK switch demo with Codewarrior 5.0. I get the following error message from the linker: "L1936: ELF output: Burner Error: Could not open the Link Burner Output file." I can compile the SMAC examples and debug them no problem. I tried to adjust some of the settings in Codewarrior to match the SMAC settings without success. (I'm new to Codewarrior and would like to concentrate on the application, not the tools) What do I adjust to get a successful compile and link of the EVK Switch demo?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

899件の閲覧回数
DARCY_R
Contributor I
I think I found the problem. In the linker panel of the Target Settings, the whole panel is squashed. I imagine this is because of my particular video monitor settings. Anyway, the last radio button (Absolute, Single-File Assembly Project) is truncated and squashed together with the next line (Application Filename).  It looked as if they were the same item. (Looking similar to the first radio button entry, (Use Custom PRM file).
 
Anyway the Application Filename referred to a non-existant path.
 
I tried installing the whole works on another PC and got the same result. Changing to a correct path for the output now works fine.
 
Many of the Target Settings panels are messed up on my machine. Some of the right edge buttons on the OSEK Sysgen panel are not even visible...
 
0 件の賞賛
返信

899件の閲覧回数
CrasyCat
Specialist III
Hello Which OS are you running on your host machine? CrasyCat
0 件の賞賛
返信