MC13211 VS MC13213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13211 VS MC13213

1,669件の閲覧回数
e2saleh
Contributor I

I'm was using smac in MC13213 where the device goes to sleep mode (stop mode 3) and wakes up via a keyboard interrupt (PORTA/KBI), it worked fine. I changed the chip to MC13211 which has no difference except the RAM/ROM size.. The problem I faced after using the MC13211 chip is that I found there is a 600uA current draw in the sleep mode which is supposed to be less than 1uA!!! The same code on the same hardware draws 1uA if I use MC13213,, but when I use MC13211 the current start ramping from 50uA up to 600uA !! could anyone explain what is going.

Regards

Ehab
ラベル(1)
0 件の賞賛
返信
1 返信

795件の閲覧回数
FPatrick
Contributor I
Hello e2saleh,
 
I think it is 99%, that is caused by any floating pins. Even it is inside the MCU (not pins outside).
Check every port declared to output or input with pullup enabled.
I faced the sam issue yesterday.
 
Hope it helps.
 
Regards,
Peter
0 件の賞賛
返信