MC13211 VS MC13213

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC13211 VS MC13213

1,664 次查看
e2saleh
Contributor I

I'm was using smac in MC13213 where the device goes to sleep mode (stop mode 3) and wakes up via a keyboard interrupt (PORTA/KBI), it worked fine. I changed the chip to MC13211 which has no difference except the RAM/ROM size.. The problem I faced after using the MC13211 chip is that I found there is a 600uA current draw in the sleep mode which is supposed to be less than 1uA!!! The same code on the same hardware draws 1uA if I use MC13213,, but when I use MC13211 the current start ramping from 50uA up to 600uA !! could anyone explain what is going.

Regards

Ehab
标签 (1)
0 项奖励
回复
1 回复

790 次查看
FPatrick
Contributor I
Hello e2saleh,
 
I think it is 99%, that is caused by any floating pins. Even it is inside the MCU (not pins outside).
Check every port declared to output or input with pullup enabled.
I faced the sam issue yesterday.
 
Hope it helps.
 
Regards,
Peter
0 项奖励
回复