LCD drive problem - MC09S08LL16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LCD drive problem - MC09S08LL16

1,643 次查看
Javercis
Contributor I
Hi everyone,
I have a LCD drive problem.

I want to drive a 8x24 LCD drive. LCD voltage is 3V and f = 51 Hz. via MC09S08LL16 microcontrller.

Problem;
When I set more than 3 segment on the same Frontplane the other segments are also appear but they are weak.

If I set only one segment this segment is also weak.
1 to 3 segment is working fine. The position of the segment doesnt care, but they must be on the same FP.

I hope someone can help me.





Message Edited by NLFSJ on 2009-02-02 06:24 AM
标签 (1)
0 项奖励
回复
2 回复数

734 次查看
jag
Contributor IV
Try to put some external pullups on the lines. Bye Jack
0 项奖励
回复

734 次查看
Javercis
Contributor I
thanks for advise,

I change the configuration from Charge Pump enable to resistor devider enable and the problem is gone.

I hope the solution is not temporay..
Thanks ain for your attention...


0 项奖励
回复