Hello! I search for a LCD Driver Library. The Microcontroller i have is Freescale MC9S08dz60 and the Grafik LCD has 160*80dot with the T6963c Grafikcontroller.
Have anybody something librays?
Thanks Markus
Hi Markus,
yes, I'm german, but for other readers here, I'll answer in english language.
I have found the files at http://www.sctec.com.br/content/view/85/46/ some days ago.
But I have no more information about that, no hardware, never compiled by myself.
You have to find out more by yourself, sorry.
Also, i know some other sources for interface Freescale uP <---> T6963 graphic controller.
1.) My preference:
This is "DRM008" , "Alarm Control Panel Reference Design" from Oliver Thamm.
You can download complete sourcecode & documentation from
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDHCS12ACP
The project ist for HCS12, but well documented, and written in C.
See file "t6963.c"
2.) A "bean" for Processor Expert is also available ...
http://www.processorexpert.com/package_info.php?pac_id=396&tpl=mc__package_info.html&&s_bea_id=&&s_rel_id[]=4&&&&&&&s_bean_name=&&&FormTable_Sorting=6&FormTable_Sorted=&&Formtable_Page=&&Formmcus_Page=3&Formmcus_Page=2
3.)
Another source (german language) for questions about T6963 is http://www.mikrocontroller.net/ forum.
Search for T6963:
http://www.mikrocontroller.net/forum/mikrocontroller-elektronik?filter=T6963
But the discussions there should be handled with care, because sometimes not really accurate.
Klaus
A copy of complete project information HW+SW about "Alarm Control Panel Reference Design" for HCS12 is available at
http://elmicro.com/hc12web/acprd/index.html
A book about HCS12 uP , little expensive, is ISBN 10: 1435486145 ISBN 13: 9781435486140
Another one is ISBN-10: 0136072291 ISBN-13: 978-0136072294 , again little expensive.
See ebay or amazon for details. Search for "HCS12" .
German book from Oliver Thamm is no more available ; maybe you can find a used one ISBN-10: 3446217754 ISBN-13: 978-3446217751
A book about HCS08 is ISBN-10: 1419685929 ISBN-13: 978-1419685927
Search amazon for "HCS08"
Hallo, aus dem letzten Satz nehme ich an du sprichst deutsch?? ich verstehe die Lib nicht- speziell di Pinzuordnung:
#ifndef lcdg_cd
#define lcdg_cd P2OUT_bit.P2OUT_1 was bedeutet P2OUT_bit.P2OUT_1, etwa das Port 2
Pin1 auf ausgang ist???
#define lcdg_cd_dir P2DIR_bit.P2DIR_1 was wird hier gemacht?
#endif
#ifndef lcdg_rd
#define lcdg_rd P2OUT_bit.P2OUT_3
#define lcdg_rd_dir P2DIR_bit.P2DIR_3
#endif
#ifndef lcdg_wr
#define lcdg_wr P2OUT_bit.P2OUT_2
#define lcdg_wr_dir P2DIR_bit.P2DIR_2
#endif
#ifndef lcdg_ce
#define lcdg_ce P2OUT_bit.P2OUT_0
#define lcdg_ce_dir P2DIR_bit.P2DIR_0
#endif
#ifndef lcdg_dados_out Sind das die Datenbits D0-D7?
#define lcdg_dados_dir P1DIR was wird hier gmacht?
#define lcdg_dados_out P1OUT ....und hier ein ganzer Port auf low....
#define lcdg_dados_in P1IN und hier wieder auf high gesetzt
#endif
Danke
Markus