Is possible to program a MC9S08GT60CFB with USB-ML-MON08?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is possible to program a MC9S08GT60CFB with USB-ML-MON08?

跳至解决方案
1,789 次查看
TG
Contributor I

Hello everybody.

 

I want to know if it's possible to program/debug a MC9S08GT60CFB device with a USB-ML-MON08 interface. I think that the answer is no, but i don't know if exists any adapter or something like that to make it possible.

 

Thanks.

标签 (1)
0 项奖励
回复
1 解答
822 次查看
peg
Senior Contributor IV

Hello and welcome to the fora, TG,

 

Your USB-ML-MON08 is only good for HC08 devices (i.e. one that use a MON08 interface)

 

You will  need a USB-ML-12 or similar BDM type adapter to programme S08 devices (one of which is the 9S08GT60)

 

You might also consider an OSBDM as discussed in the community project forums here.

 

Message Edited by peg on 2009-07-16 07:37 AM

在原帖中查看解决方案

0 项奖励
回复
2 回复数
823 次查看
peg
Senior Contributor IV

Hello and welcome to the fora, TG,

 

Your USB-ML-MON08 is only good for HC08 devices (i.e. one that use a MON08 interface)

 

You will  need a USB-ML-12 or similar BDM type adapter to programme S08 devices (one of which is the 9S08GT60)

 

You might also consider an OSBDM as discussed in the community project forums here.

 

Message Edited by peg on 2009-07-16 07:37 AM
0 项奖励
回复
822 次查看
TG
Contributor I

Ok, thanks for your help and the fast reply peg.

 

0 项奖励
回复