Is necessary more than 1 ADC to measure AC voltage, Current and frequency?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is necessary more than 1 ADC to measure AC voltage, Current and frequency?

ソリューションへジャンプ
1,263件の閲覧回数
Braulio_Cespede
Contributor III

Hello everyone.

 

I have to work in a Project, but I not sure about this.

I think, It could be make with one, but to be sure can you tell me?.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,004件の閲覧回数
eduardo_viramon
NXP Employee
NXP Employee

Braulio,

If you plan to measure current and voltage, you need at least one ADC channel per each of those variables. Frequency is calculated from either of the current or voltage measurements (much easier based on the voltage).

The reference design in the link below has full information on how to implement a single-phase power meter. This should give you all the info you need:

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/DRM133.pdf?fsrch=1&sr=11

Regards,

Eduardo V.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,005件の閲覧回数
eduardo_viramon
NXP Employee
NXP Employee

Braulio,

If you plan to measure current and voltage, you need at least one ADC channel per each of those variables. Frequency is calculated from either of the current or voltage measurements (much easier based on the voltage).

The reference design in the link below has full information on how to implement a single-phase power meter. This should give you all the info you need:

http://cache.freescale.com/files/microcontrollers/doc/ref_manual/DRM133.pdf?fsrch=1&sr=11

Regards,

Eduardo V.

0 件の賞賛
返信
1,004件の閲覧回数
Braulio_Cespede
Contributor III

Thanks you.

0 件の賞賛
返信