Is it necessary to register CodeWarrior Special Edition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it necessary to register CodeWarrior Special Edition

2,556件の閲覧回数
robert2000
Contributor II
Hello
I download CodeWarrior Special edition for HC(S)08 /ColdfireV1 Version 6.2. This a free software but the software is requesting to Register. I don't understand what I should do.
Thanks for your help
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,365件の閲覧回数
NLFSJ
Contributor III
The special edition licenses do not require registration.   They are active upon installation. 
Have you placed the license.dat file in the directory where you installed the software?
0 件の賞賛
返信

1,365件の閲覧回数
robert2000
Contributor II
HelloNina
I am able to access the software which is working well. But it's time limited: only one month.
I am not sure to understand your comment but I give the same directory for the installation and 
the license.dat file . Is that correct?
Robert
0 件の賞賛
返信

1,365件の閲覧回数
J2MEJediMaster
Specialist I
We've had a glitch where people are getting the Evaluation Edition of the CodeWarrior software when they download the Special Edition. The Evaluation edition is similar to the Special Edition, except that it's fully featured for one month. Once the trial period ends, it becomes the Special Edition, with its code size limits. See FAQ-28561 for a little more detail. And no, you don't have to register the software, unless you want to purchase the full features after the temporary license expires.

---Tom
0 件の賞賛
返信

1,365件の閲覧回数
robert2000
Contributor II
Hello Tom
 
Thanks a lot for this info.
So , I have just to keep the software and, I will get the special Edition after one month.
 
Best Regards
Robert
0 件の賞賛
返信