In which mode  MC1321x should operate to increase the battery life time?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In which mode  MC1321x should operate to increase the battery life time?

1,226件の閲覧回数
lekkal
Contributor I
Hi All,
 
 
I have designed a MC13213 board which is suppose to work with coin cell battery (CR2354,500mAh) atleast for 12months.When it is in communication with other module i.e. either in Tx or Rx it is drawing ~50mA and in idle mode current is 7mA.If I keep the module continuously in idle mode then battery life time will be just 3days (500/7 = 72hours = 3days). If I use two AA batteries life time will be 11days(1800/7 = 257hours = 11days). In which mode  should it operate to increase the battery life time? Please give me the complete details off different modes like current,RAMstatus,I/O ports status and etc
 
 
 
Thanks & Regards,
Lekkal
ラベル(1)
0 件の賞賛
返信
1 返信

594件の閲覧回数
J2MEJediMaster
Specialist I
Low power consumption topics have been discussed in these forums before. If you haven't already, try using the search funtion (bottom left text insertion box) and enter the phrase "low power mode". There are several threads with usigful information.

---Tom

0 件の賞賛
返信