If the pin 72 marked with flag opening of MC13213 need to be connected to ground?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If the pin 72 marked with flag opening of MC13213 need to be connected to ground?

1,829件の閲覧回数
Relax
Contributor I
The internal oscillator is unable to work. I guess it's the problem of pin 72. So I'd like to confirm that if the pin 72 marked with flag opening of MC13213 need to be connected to ground?
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

905件の閲覧回数
Relax
Contributor I
There are still something wrong with my PCB. When the pin 72 is connnected to ground, the internal oscillator is unable to work, but once it is cut off from the ground, the oscillator is running.
So could you tell me the reason for the problem? or Is there some other fault in my PCB itself?
0 件の賞賛
返信

905件の閲覧回数
peg
Senior Contributor IV
Hi,
 
You have checked (measured) for shorts between pins and the flag?
If you look at the pin designations you will see there is no other main ground connection other than the flag. It needs to be connected.
 
0 件の賞賛
返信

905件の閲覧回数
peg
Senior Contributor IV
Hi Relax,
 
Most certainly it does!
 
0 件の賞賛
返信